XBARA Missing from SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XBARA Missing from SDK

ソリューションへジャンプ
2,542件の閲覧回数
OnoFame
Contributor II

,

XBARA is not included in the SDK for MKV44. There is a similar post here:

Solved: Re: MKV44 SDK 2.8.0 missing XBARA Driver - NXP Community

Could you please resolved this? You are definitely not expecting us to use the sdk for MKV46 on the MKV44 platform, are you? 

0 件の賞賛
返信
1 解決策
2,537件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I downloaded the 2.8.0 SDK for the MKV44F128xxx16 and I found the xbara drivers inside the following route …devices/MKV46F16/drivers.

Could you please give it a try?

Best regards, Daniel.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,538件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

I downloaded the 2.8.0 SDK for the MKV44F128xxx16 and I found the xbara drivers inside the following route …devices/MKV46F16/drivers.

Could you please give it a try?

Best regards, Daniel.

0 件の賞賛
返信
2,527件の閲覧回数
OnoFame
Contributor II

Thanks, I found it and I have copied it into the project directory:

From ... C:\Users\"myusername"\mcuxpresso\02\SDKPackages\SDK_2_8_0_MKV46F128xxx16\devices\MKV46F16\drivers

to ...

C:\..\ProjectDirectory\drivers

Thanks a million. I hope there will be a release of possibly new version with Xbara included within the MCUXpresso IDE's SDK management interface.

0 件の賞賛
返信
2,531件の閲覧回数
OnoFame
Contributor II

Thanks for responding, Do you mean I should look some where in Windows Explorer? (This is the first product based around MCUXpresso platform and all I see is this interface where you right click and then go manage SDK... This is where XBARA is missing from).

OnoFame_0-1660634049067.png

 

0 件の賞賛
返信