MKV44 SDK 2.8.0 missing XBARA Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKV44 SDK 2.8.0 missing XBARA Driver

ソリューションへジャンプ
2,858件の閲覧回数
katha
Contributor II

Hello,

I try to add the XBARA driver to my MKV44 project, but I cant find it in the SDK. In SDK for MK64 2.8.2 it is available. Is there any reason?

Thanks a lot and kind regards

0 件の賞賛
返信
1 解決策
2,848件の閲覧回数
Masmiseim
Senior Contributor I

I can not explain why they are missing for the KV44, however they are included in the SDK package for the KV46. This should also work for the KV44. I would give it a try

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,849件の閲覧回数
Masmiseim
Senior Contributor I

I can not explain why they are missing for the KV44, however they are included in the SDK package for the KV46. This should also work for the KV44. I would give it a try

0 件の賞賛
返信
2,825件の閲覧回数
katha
Contributor II

Is there a possibility to add it soon?

Whats about the ftm driver? In reference manual it has an extra section besides the eFlexPWM

Regards

0 件の賞賛
返信