Will Kinetis Design Studio support OSJTAG?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will Kinetis Design Studio support OSJTAG?

Jump to solution
4,364 Views
kenansun
Contributor II

Hi,

I'm very interested in this new IDE: Kinetis Design Studio. It has no code limits and it is equipped with PEx, MQX, etc.

But I don't see if it has built-in debug mode for OSJTAG, just like what CodeWarrior does.

Many Kinetis TWR boards have this debug interface so  I'm wondering if Freescale will support it?

If not, we have to use CW or buy a debugger.:smileysad:


Many thanks

0 Kudos
Reply
1 Solution
3,899 Views
mjbcswitzerland
Specialist V

Hi

See Codewarrior will no longer be supporting new Kinetis parts????

I can't imagine that there will be no OSJTAG support, otherwise there would be no point in KDS. It should be available in the next few days so we will know for sure then but I would put bets on the same interfaces as CW has.

Regards

Mark

View solution in original post

0 Kudos
Reply
5 Replies
3,899 Views
BlackNight
NXP Employee
NXP Employee

KDS supports GDB with OpenOCD, Segger and P&E. And P&E supports OSJTAG. Therefore, OSJTAG is supported with KDS, so you can for example a Kinetis Tower board with KDS: simply select P&E GDB in KDS. Similar what is present in CodeWarrior today where OSJTAG is supported with P&E as well.

Just one correct: KDS does not come with MQX, but you can use MQX with KDS.

Erich

3,899 Views
kenansun
Contributor II

Hey Erich,

Your blog is fantastic, and it does help me a lot with PEx and Eclipse:smileyhappy:

Thanks for your reply, and the correction!

In fact, I know that OSJTAG is supported by P&E, but I was just wondering if the P&E server will be integrated in KDS_IDE. Because the P&E server is also charged. Well, thanks for Mark's link, I'm no longer worried about that.

Kenan

0 Kudos
Reply
3,899 Views
BlackNight
NXP Employee
NXP Employee

Hi Kenan,

The GDB server from P&E inside KDS is free of charge and unlimited. Beside of that, you have options including USBDM (see Using USBDM with Kinetis Design Studio).

Erich

0 Kudos
Reply
3,900 Views
mjbcswitzerland
Specialist V

Hi

See Codewarrior will no longer be supporting new Kinetis parts????

I can't imagine that there will be no OSJTAG support, otherwise there would be no point in KDS. It should be available in the next few days so we will know for sure then but I would put bets on the same interfaces as CW has.

Regards

Mark

0 Kudos
Reply
3,899 Views
kenansun
Contributor II

Hi Mark,

Apologize for this delayed response!

I didn't imagine that so many people might have the similar problem as I did.. I should have searched for answers before asking them:smileysad:

Anyway thanks for your helpful answer!

Kenan

0 Kudos
Reply