Wich MCU (KInetis ARM) to control LCD-TFT via 8080 interface ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wich MCU (KInetis ARM) to control LCD-TFT via 8080 interface ?

Jump to solution
5,433 Views
joelesco
Contributor III

Hi everybody !

I'm a new member and i'm so happy to enter in the Freescale community ! I'm french and my english is not really good but i'll try to explain clearly my problem !

I want to choose the good kinetis MCU  to control my LCD-TFT display ! This display as an integer controlleur ( SSD1963 from Solomon) and could discuss with MCU with 8080 and 6800 interface ! I'm looking for a MCU which can do that but I found nothing and I supppose that it could be possible !

I hope someone have already use this kind of interface with a Kinetis and could give me some indication !

Thanks a lot !

1 Solution
3,423 Views
hectorsanchez
Contributor IV

Hi Joe,

Hope i get this right, but the SSD1963 is a LCD Controller that uses parallel interface to make the interface with processors and maybe via SPI.

Said this, you can use any processor to make the TFT work, the Kinetis can be interfaced easily with the FlexBus.

I recommend you to check the K70 Family because it has an internal LCD controller which does not require an external LCD controller like the SSD1963 from Solomon.

Here is the link if you want to know more about the K70 Family and see if this device is the one you need:

http://www.freescale.com/files/32bit/doc/fact_sheet/KNTSK70FS.pdf

If you have more questions feel free to post them, I'll be glad to answer them

Hector

View solution in original post

0 Kudos
Reply
10 Replies
3,423 Views
weblar
Contributor V

Hi Joe,

You can use the FlexBus on a device like the K60 to control the LCD in 6800 mode - that's how I'm interfacing to an SSD1963.

At present, I'm using a 150MHz K60FN1M0 device which works brilliantly for what I want. The LCD update rate via FlexBus is very very fast (compared with GPIO bit banging).

3,423 Views
joelesco
Contributor III

Sorry to re-open the topic ! But do you think if I use the FlexBus with a K20 at 75Mhz is okay for the LCD ?

Thanks again !

0 Kudos
Reply
3,423 Views
LuisCasado
NXP Employee
NXP Employee

Hi Jeremie,

I successfully tested an smart LCD with build-in controller IL9341 what only supports 8080 mode connected to K20@100 Mhz connected to Kinetis FlexBus what doesn't support 8080 mode.

CS LCD connected to GPIO or grounded

RS connected to GPIO to select command/data (Optional connected to Axx flexbus address pin)

LCD_RD connected to FlexBus CSx pin

LCD_WR connected to Flexbus CSy pin

LCD_DATA  D0 to D15 connected to FB_AD16  to FB_AD31

You have to configure two FlexBus CS pins with its own memory space. Write and RD flexbus operations will write/read the LCD controller.

Best Regards,

3,423 Views
rqbh
Contributor III

Hi, Luis

I'm facing that problem now, with a K22F120M and IL9806 using flexbus, can you share your flexbus configure code or give some more detail information ?

0 Kudos
Reply
3,423 Views
joelesco
Contributor III

Great ! I alway asking me if it's possible to connect a parallel Bus with GPIO !  you seems to says that is possible, isn it ?

thank again !

0 Kudos
Reply
3,423 Views
mjbcswitzerland
Specialist V

Hi

LCDs with inbuilt controllers (as the one that is the subject here) can be controlled by bit-banging but the FlexBus is the most efficient:

The followig video shows such an LCD being driven by the Coldfire Flexbus (equivelent to Kinetis)

cf-tower_0003.wmv - YouTube

The SLCD interface in the K40 (for example) is used for segment display - see the following video:

http://www.youtube.com/watch?v=nm2DmZv1rj8

As comparison, the LCD is seen here being bit-banged (using a different processor type but again equivelent):

IDM-L35-Part2.wmv - YouTube

Regards

Mark

0 Kudos
Reply
3,423 Views
perlam_i_au
Senior Contributor I

Hi Joe:

For use this specific controller (SSD1963) you can use any Kinetis product or if you prefer, you can use K40 which has dedicated module for LCD controller integrated.

0 Kudos
Reply
3,424 Views
hectorsanchez
Contributor IV

Hi Joe,

Hope i get this right, but the SSD1963 is a LCD Controller that uses parallel interface to make the interface with processors and maybe via SPI.

Said this, you can use any processor to make the TFT work, the Kinetis can be interfaced easily with the FlexBus.

I recommend you to check the K70 Family because it has an internal LCD controller which does not require an external LCD controller like the SSD1963 from Solomon.

Here is the link if you want to know more about the K70 Family and see if this device is the one you need:

http://www.freescale.com/files/32bit/doc/fact_sheet/KNTSK70FS.pdf

If you have more questions feel free to post them, I'll be glad to answer them

Hector

0 Kudos
Reply
3,423 Views
joelesco
Contributor III

Thank you Hector !

I already have the Display with the controller that's why i'll use the FlexBus that seems to be the same that FSMC with STM32 !

This forum looks great ! I'm going to feel comfortable !


3,423 Views
hectorsanchez
Contributor IV

I'm glad i was able to help you.

Hope to see you in the forum more often :smileyhappy:

0 Kudos
Reply