Why do I get USBRST interrupt right after enabling it?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why do I get USBRST interrupt right after enabling it?

1,941件の閲覧回数
flaggermusman
Contributor I

Hello all,

I'm trying to get familiar with USBOTG module in Kinetis K60D512 MCU and I'm encountering some issues I'm not sure about.

First I don't understand why there's an USB interrupt signalizing set USBRST right after I enable only this interrupt source before pulling up D+ to signalize attached device.

The code I use is the following:

///******* CLOCK configuration *****************

// Configure USB to be clocked from PLL0

SIM->SOPT2 |= SIM_SOPT2_PLLFLLSEL_MASK |SIM_SOPT2_USBSRC_MASK;

// Configure USB divider to be 2 (SYSCLOCK = 96MHz)

// USBclk = PLLclk × [ (USBFRAC+1) / (USBDIV+1) ]

SIM->CLKDIV2 = SIM_CLKDIV2_USBDIV(1);

// Enable USB-OTG IP clocking

SIM->SCGC4 |= SIM_SCGC4_USBOTG_MASK;

///********* USB configuration **********

// Enable interrupts

NVIC_EnableIRQ(USB0_IRQn);

// Configure enable USB regulator for device

SIM->SOPT1 |= SIM_SOPT1_USBREGEN_MASK;

// enable USB module

USB0->CTL |= USB_CTL_USBENSOFEN_MASK;

// Module reset

USB0->USBTRC0 |= USB_USBTRC0_USBRESET_MASK;

// set BDT address

USB0->BDTPAGE1 = (uint8_t) ((uint32_t)&bdt >> 8);

USB0->BDTPAGE2 = (uint8_t) ((uint32_t)&bdt >> 16);

USB0->BDTPAGE3 = (uint8_t) ((uint32_t)&bdt >> 24);

// enable control of pullups

USB0->OTGCTL |= USB_OTGCTL_OTGEN_MASK;

// enable weak pull-downs and turn on transceiver

USB0->USBCTRL |= USB_USBCTRL_PDE_MASK;

USB0->USBCTRL &= ~USB_USBCTRL_SUSP_MASK;

// clear all USB ISR flags

USB0->ISTAT = 0xFF;

// enable USB RESET interrupt

USB0->INTEN |= USB_INTEN_USBRSTEN_MASK;

/// !!!! This chunk is executed from an interrupt handler for a button:

// signalize attached device

USB0->CONTROL |= USB_CONTROL_DPPULLUPNONOTG_MASK;

USB0->OTGCTL |= USB_OTGCTL_DPHIGH_MASK;

Right after line USB0->INTEN |= USB_INTEN_USBRSTEN_MASK there is an interrupt on USB0_IRQ signalizing USBRST event even though the pullup od D+ is off (I could check in OBSERVE reg). But when I press the button and enter its interrupt handler then the regular USBRST event occurs because Windows signalizes new USB device (of course unsuccessfully installed). So is there any reason for this behavior? Getting USBRST interrupt event right after enabling interrupts? I also tried to change the configuration of USB module commenting out and changing some of the previous register configurations but the result is always the same.

Is there any documentation on the USB controller used in this kinetis I'm using? The reference manual isn't very comprehensive and I think some things would really deserve more information. USB Stack examples really doesn't cover this too.

Thanks a lot for any help.

ラベル(2)
0 件の賞賛
返信
1 返信

1,461件の閲覧回数
mjbcswitzerland
Specialist V

Buchta

1. After enabling the USB regulator it is usual to disable its standby mode (remove UVSWE bit)

2. When commanding the USB controller reset it is usual to wait for the reset to complete with

while (USB0->USBTRC0 & USB_USBTRC0_USBRESET_MASK) {                     // wait for the reset to complete

}

3. Before enabling the D+ pull up it is recommended to set 0x40 to USB0->USBTRC0. This is an undocumented bit but it is set in most code examples and ensures correct pull-up operation (for some reason).

4. When both bus lines are low for 2.5us it is detected as a USB reset. Therefore I think you should only enable the RST interrupt once you have actually pulled up the D+ line (for FS mode) and you will need to clear the pending interupt before as well.

Regards

Mark

http://www.utasker.com/kinetis.html

0 件の賞賛
返信