Termination for SPI Clock at 2MHZ for MK70FN1M0VMJ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Termination for SPI Clock at 2MHZ for MK70FN1M0VMJ12

1,188 Views
puspamnayak
Contributor III


Hi,

I am using MK70FN1M0VMJ12 in my project and SPI clock & data may go speed up to 2MHz so want to know does it need a termination. If its required then what will be the recommned value for the termination

Please reply at earliest

Thanks and regards,

Puspam Nayak

Tags (1)
0 Kudos
Reply
1 Reply

1,071 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Puspam Nayak,

The maximum frequency of the DSPI could be up to 30MHz.

In my opinion, it doesn't need set a termination when the frequency of DSPI operation is 2MHz.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply