Where to find chip-specific information for KL17 DACREF?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to find chip-specific information for KL17 DACREF?

Jump to solution
1,226 Views
pcpro178
Contributor III

I'm using the MKL17Z256VLH4.  Section 25.5 of the reference manual states, "The 12-bit DAC module can select one of the two reference inputs—DACREF_1 and DACREF_2 as the DAC reference voltage, Vin by C0 [DACRFS]. See the chip-specific DAC information to determine the source options for DACREF_1 and DACREF_2."

I've searched through the reference manual and datasheet.  Where do I find the chip-specific information for the DACREF source options?

Labels (1)
0 Kudos
Reply
1 Solution
1,104 Views
miduo
NXP Employee
NXP Employee

Hi,


The references for DAC are mapped as:

DACREF_1: VREFH
DACREF_2: VDDA

This information can been found at Table 2-13. Analog reference options of the reference manual.


View solution in original post

1 Reply
1,105 Views
miduo
NXP Employee
NXP Employee

Hi,


The references for DAC are mapped as:

DACREF_1: VREFH
DACREF_2: VDDA

This information can been found at Table 2-13. Analog reference options of the reference manual.