Where to find chip-specific information for KL17 DACREF?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where to find chip-specific information for KL17 DACREF?

ソリューションへジャンプ
2,008件の閲覧回数
pcpro178
Contributor III

I'm using the MKL17Z256VLH4.  Section 25.5 of the reference manual states, "The 12-bit DAC module can select one of the two reference inputs—DACREF_1 and DACREF_2 as the DAC reference voltage, Vin by C0 [DACRFS]. See the chip-specific DAC information to determine the source options for DACREF_1 and DACREF_2."

I've searched through the reference manual and datasheet.  Where do I find the chip-specific information for the DACREF source options?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,886件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,


The references for DAC are mapped as:

DACREF_1: VREFH
DACREF_2: VDDA

This information can been found at Table 2-13. Analog reference options of the reference manual.


元の投稿で解決策を見る

1 返信
1,887件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,


The references for DAC are mapped as:

DACREF_1: VREFH
DACREF_2: VDDA

This information can been found at Table 2-13. Analog reference options of the reference manual.