Where to find chip-specific information for KL17 DACREF?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where to find chip-specific information for KL17 DACREF?

跳至解决方案
2,023 次查看
pcpro178
Contributor III

I'm using the MKL17Z256VLH4.  Section 25.5 of the reference manual states, "The 12-bit DAC module can select one of the two reference inputs—DACREF_1 and DACREF_2 as the DAC reference voltage, Vin by C0 [DACRFS]. See the chip-specific DAC information to determine the source options for DACREF_1 and DACREF_2."

I've searched through the reference manual and datasheet.  Where do I find the chip-specific information for the DACREF source options?

标签 (1)
0 项奖励
回复
1 解答
1,901 次查看
miduo
NXP Employee
NXP Employee

Hi,


The references for DAC are mapped as:

DACREF_1: VREFH
DACREF_2: VDDA

This information can been found at Table 2-13. Analog reference options of the reference manual.


在原帖中查看解决方案

1 回复
1,902 次查看
miduo
NXP Employee
NXP Employee

Hi,


The references for DAC are mapped as:

DACREF_1: VREFH
DACREF_2: VDDA

This information can been found at Table 2-13. Analog reference options of the reference manual.