What will be the extreme values of ADC result when resolution is 16 bit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What will be the extreme values of ADC result when resolution is 16 bit?

1,142 次查看
pramodk_g_
Contributor III

Hi everyone,

                                 When I  run ADC example for TWR K60D100M , it is found that adc result is 32267 when probed to 3.3V and 65523 or 34 etc. for 0v . Adc resolution used in the code is 16bit, so the extreme value should be 65535 and 0 (For 3.3V and 0V ), is it correct?. Is there any change need to achieve this or I went wrong somewhere?

Please help..

Thanks

Pramod

标记 (4)
0 项奖励
回复
1 回复

921 次查看
hectorsanchez
Contributor IV

Hi Pramod,

I suggest you to check this thread: Re: ADC on TWRK60N512 ?
Keep me informed if this helped you.

Best Regards,

Hector Sanchez

0 项奖励
回复