What are the differences between K61 and K70 microcontrollers?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What are the differences between K61 and K70 microcontrollers?

跳至解决方案
1,890 次查看
kaitav
Contributor III

Hi,

We are planning to select either K61 and K70 microcontroller for our next design and would want to know the major differences between the two or the differences worth considering. We are looking at the 256-pin BGA package for both.

I went through the documentation and Kinetis MCU Selection guide quickly to find that K70 additionally has a Graphic LCD controller. Apart from this, I was not able to see any major differences between the two. Both K61 and K70 have DDR memory controller in their 256-pin BGA packages, and we want to use it in our design. Specifically to DDR controller, is there any difference between the DDR controller of K61 and that of K70?

Any help would be much appreciated.

Thanks,

Kaitav

标签 (1)
0 项奖励
回复
1 解答
1,618 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Kaitav Sapre,


DDR controller specifications are absolutely identical.

I checked the both datasheets http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K61P256M120SF3.pdf and http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K70P256M120SF3.pdf?fasp=1&WT_TYPE=D...

and the only difference between these both MCUs is the Graphic LCD controller for K70.


I´m also attaching you for your summarize both of them :

rozdil.png

rozdil2.png


Best Regards,

Iva

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,619 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Kaitav Sapre,


DDR controller specifications are absolutely identical.

I checked the both datasheets http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K61P256M120SF3.pdf and http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K70P256M120SF3.pdf?fasp=1&WT_TYPE=D...

and the only difference between these both MCUs is the Graphic LCD controller for K70.


I´m also attaching you for your summarize both of them :

rozdil.png

rozdil2.png


Best Regards,

Iva

0 项奖励
回复
1,618 次查看
kaitav
Contributor III

Hi Iva,

Thanks for the confirmation. :smileyhappy:

Regards,

Kaitav Sapre

0 项奖励
回复