What are the differences between K61 and K70 microcontrollers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the differences between K61 and K70 microcontrollers?

Jump to solution
2,564 Views
kaitav
Contributor III

Hi,

We are planning to select either K61 and K70 microcontroller for our next design and would want to know the major differences between the two or the differences worth considering. We are looking at the 256-pin BGA package for both.

I went through the documentation and Kinetis MCU Selection guide quickly to find that K70 additionally has a Graphic LCD controller. Apart from this, I was not able to see any major differences between the two. Both K61 and K70 have DDR memory controller in their 256-pin BGA packages, and we want to use it in our design. Specifically to DDR controller, is there any difference between the DDR controller of K61 and that of K70?

Any help would be much appreciated.

Thanks,

Kaitav

Labels (1)
0 Kudos
Reply
1 Solution
2,292 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Kaitav Sapre,


DDR controller specifications are absolutely identical.

I checked the both datasheets http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K61P256M120SF3.pdf and http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K70P256M120SF3.pdf?fasp=1&WT_TYPE=D...

and the only difference between these both MCUs is the Graphic LCD controller for K70.


I´m also attaching you for your summarize both of them :

rozdil.png

rozdil2.png


Best Regards,

Iva

View solution in original post

0 Kudos
Reply
2 Replies
2,293 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Kaitav Sapre,


DDR controller specifications are absolutely identical.

I checked the both datasheets http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K61P256M120SF3.pdf and http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K70P256M120SF3.pdf?fasp=1&WT_TYPE=D...

and the only difference between these both MCUs is the Graphic LCD controller for K70.


I´m also attaching you for your summarize both of them :

rozdil.png

rozdil2.png


Best Regards,

Iva

0 Kudos
Reply
2,292 Views
kaitav
Contributor III

Hi Iva,

Thanks for the confirmation. :smileyhappy:

Regards,

Kaitav Sapre

0 Kudos
Reply