Watchdog for S9KEAZN8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog for S9KEAZN8

Jump to solution
1,944 Views
johns_chuang
Contributor III

Hello,

Does the Watchdog of S9KEAZN8 have the following features?

1. No dependence between watchdog time base and controller time base.
2. The watchdog is activated automatically.
3. It must not be possible to stop or reconfigure the watchdog outside the
4. Initialization phase of the watchdog.

 

Thanks for your help.

Johns

 

 

0 Kudos
Reply
1 Solution
1,934 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @johns_chuang 

1. Watchdog timer works independently, it has an independent 1kHz oscillator.

2. Yes, Watchdog timer is inabled immediatley but it is disbaled during debug mode.

3 & 4? WDOG_CS1[UPDATE] could allow updates on the configuration without forcing a reset on the mcu.

You can find more information on chapter 16 of the reference manual.

Let me know if this answers your questions.

Best Regards, Miguel.

View solution in original post

2 Replies
1,924 Views
johns_chuang
Contributor III

Hi Miguel

Thanks for your reply, it's very helpful for me.

Johns

0 Kudos
Reply
1,935 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @johns_chuang 

1. Watchdog timer works independently, it has an independent 1kHz oscillator.

2. Yes, Watchdog timer is inabled immediatley but it is disbaled during debug mode.

3 & 4? WDOG_CS1[UPDATE] could allow updates on the configuration without forcing a reset on the mcu.

You can find more information on chapter 16 of the reference manual.

Let me know if this answers your questions.

Best Regards, Miguel.