Watchdog Interrupt then Reset CPU configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog Interrupt then Reset CPU configuration

ソリューションへジャンプ
1,176件の閲覧回数
gschelotto
Contributor V

Hi,

I'm not able to configure the Watchdog using PE on MKE02Z in order to interrupt and then Reset the CPU as shown:

Untitled.png

After PE code generation INT_WDOG_EWM is not listed in vector table nor at Events.c.Before a WDG reset is performed I need to save some variables in a non volatile memory. How can I do this?

regards,

gaston

0 件の賞賛
返信
1 解決策
1,021件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello,

Once you select the Wdog component, you must go to Events tab and select "generate code" on OnWatchDog option in order to create the ISR entry that will be called once watchdog timeout occurs:

Events tab.jpg

Generate code.jpg

Then Save changes, generate code and ISR should appear on event.c file:

/*

** ===================================================================

**     Event       :  WDog1_OnWatchDog (module Events)

**

**     Component   :  WDog1 [WatchDog_LDD]

*/

/*!

**     @brief

**         Called if watchdog time-out occurs. WatchDog must support

**         this feature and must be enabled.

**     @param

**         UserDataPtr     - Pointer to the user or

**                           RTOS specific data. The pointer passed as

**                           the parameter of Init method.

*/

/* ===================================================================*/

void WDog1_OnWatchDog(LDD_TUserData *UserDataPtr)

{

  /* Write your code here ... */

}

Hope this helps!

Regards,

Isaac

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,022件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello,

Once you select the Wdog component, you must go to Events tab and select "generate code" on OnWatchDog option in order to create the ISR entry that will be called once watchdog timeout occurs:

Events tab.jpg

Generate code.jpg

Then Save changes, generate code and ISR should appear on event.c file:

/*

** ===================================================================

**     Event       :  WDog1_OnWatchDog (module Events)

**

**     Component   :  WDog1 [WatchDog_LDD]

*/

/*!

**     @brief

**         Called if watchdog time-out occurs. WatchDog must support

**         this feature and must be enabled.

**     @param

**         UserDataPtr     - Pointer to the user or

**                           RTOS specific data. The pointer passed as

**                           the parameter of Init method.

*/

/* ===================================================================*/

void WDog1_OnWatchDog(LDD_TUserData *UserDataPtr)

{

  /* Write your code here ... */

}

Hope this helps!

Regards,

Isaac

0 件の賞賛
返信