VREF_OUT usage on KL03?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VREF_OUT usage on KL03?

1,566件の閲覧回数
chucksmith
Contributor II

Hello,  I'm a bit confused about the VREF_OUT usage on the KL03. The reference guide says we can write a 1 to REF_SEL to choose VALTHI/VALTLO as the alternate reference pair. On the KL03 does this select VREF_OUT as the (internally generated) ADC voltage reference? And if so, if we are only using VREF_OUT as the internal ADC reference, do we still need the 100nf Cap?

 

Thanks,

 

Chuck

ラベル(1)
0 件の賞賛
返信
1 返信

1,422件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Chuck,

On the KL03 does this select VREF_OUT as the (internally generated) ADC voltage reference?
Yes. You can find below information from it's Reference Manual KL03P24M48SF0RM.

Analog reference options.png

And if so, if we are only using VREF_OUT as the internal ADC reference, do we still need the 100nf Cap?
Yes.

30.1 Chip specific VREF information.png

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信