VREF_OUT usage on KL03?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VREF_OUT usage on KL03?

1,564 Views
chucksmith
Contributor II

Hello,  I'm a bit confused about the VREF_OUT usage on the KL03. The reference guide says we can write a 1 to REF_SEL to choose VALTHI/VALTLO as the alternate reference pair. On the KL03 does this select VREF_OUT as the (internally generated) ADC voltage reference? And if so, if we are only using VREF_OUT as the internal ADC reference, do we still need the 100nf Cap?

 

Thanks,

 

Chuck

Labels (1)
0 Kudos
Reply
1 Reply

1,420 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Chuck,

On the KL03 does this select VREF_OUT as the (internally generated) ADC voltage reference?
Yes. You can find below information from it's Reference Manual KL03P24M48SF0RM.

Analog reference options.png

And if so, if we are only using VREF_OUT as the internal ADC reference, do we still need the 100nf Cap?
Yes.

30.1 Chip specific VREF information.png

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply