Update firmware for MK20DN512VLL10 via CAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Update firmware for MK20DN512VLL10 via CAN

1,722 次查看
huyho
Contributor III

    We are developing a motion control board using MK20DN512VLL10, the original project is here.

    We also used Processor Expert to create CAN module then integrated to firmware. CAN communication works fine.

    We plan to update firmware via CAN, we connect a computer with a CAN controller software (ie. CANUSB ) to CAN bus, every CAN node will be received the firmware package and update automatically!

    How should we implement? Thanks a lot!

    Regards,

    Huy.

标签 (1)
0 项奖励
回复
2 回复数

1,236 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Huy Ho

Please check the documents:

KEA128 CAN Bootloader 

Kinetis Bootloader for FRDM-K64 

http://www.nxp.com/assets/documents/data/en/user-guides/KBTLDRDEMOUG.pdf 

Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,237 次查看
huyho
Contributor III

Hi Vazquez,

Thanks for your response!

Can I stand in user application mode, receive and save firmware to flash or EEPROM (via CAN) then go to bootloader mode, copy the memory to correct user application place and run it (I think this method will be better for our target)? I am going to find a way to write my hex file to flash or EEPROM. Any idea about it?

Thanks a lot!

Huy.

0 项奖励
回复