UART on kl25z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,953件の閲覧回数
aayushm
Contributor I

What is the differnce  between UART0, UART1, UART2 on kl25z ?

What is the operating voltage of RX/TX pin of kl25z ?

0 件の賞賛
返信
1 解決策
2,438件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Aayush

UART0 is a special UART module. It can support basic UART with DMA interface function, x4 to x32 oversampling of baud-rate.This module supports LIN slave operation.

The module can remain functional in VLPS mode provided the clock it is using remains enabled. It can support ISO7816.

UART1 and UART2 are basic universal asynchronous receiver/transmitter (UART) modules with DMA function support. Generally, these modules are used in RS-232, RS-485, and other communications. This module supports LIN Slave operation.

UART pins are digital. So the operation voltage depends on VDD voltage value.

Hope my reply can help you.

Best Regards

Paul

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,439件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Aayush

UART0 is a special UART module. It can support basic UART with DMA interface function, x4 to x32 oversampling of baud-rate.This module supports LIN slave operation.

The module can remain functional in VLPS mode provided the clock it is using remains enabled. It can support ISO7816.

UART1 and UART2 are basic universal asynchronous receiver/transmitter (UART) modules with DMA function support. Generally, these modules are used in RS-232, RS-485, and other communications. This module supports LIN Slave operation.

UART pins are digital. So the operation voltage depends on VDD voltage value.

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信