Trouble with K10 programming with JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble with K10 programming with JTAG

ソリューションへジャンプ
2,423件の閲覧回数
gfritz
Contributor II

Hi everyone,

I have problems to establish communication between K10 and jtag probe. I use 2 differents probe : an Olimex ARM-USB-OCD-H and a Segger JLink. Both are used with OpenOCD on Linux and windows. And with both, I obtain that same error message :

Error: JTAG scan chain interrogation failed: all zeroes

Error: Check JTAG interface, timings, target power, etc.

Error: Trying to use configured scan chain anyway...

Error: k10.cpu: IR capture error; saw 0x00 not 0x01

Is someone have an idea to manage this issue ?

Thanks in advance

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,264件の閲覧回数
gfritz
Contributor II

Hi,

Thank you for your answer. We found yesterday the problem : we forgot pull-up on NMI pin (PTA4, pin54 for K10FN1M0xxx12)...

Thank you also for your kind proposition of help

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,264件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you provide the K10 JTAG related circuit?

If yes, we could check the K10 JTAG related schematics.

Customer also could check TWR-K20D50M board schematics about JTAG related circuit design.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,265件の閲覧回数
gfritz
Contributor II

Hi,

Thank you for your answer. We found yesterday the problem : we forgot pull-up on NMI pin (PTA4, pin54 for K10FN1M0xxx12)...

Thank you also for your kind proposition of help

0 件の賞賛
返信