Trouble with K10 programming with JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble with K10 programming with JTAG

Jump to solution
2,390 Views
gfritz
Contributor II

Hi everyone,

I have problems to establish communication between K10 and jtag probe. I use 2 differents probe : an Olimex ARM-USB-OCD-H and a Segger JLink. Both are used with OpenOCD on Linux and windows. And with both, I obtain that same error message :

Error: JTAG scan chain interrogation failed: all zeroes

Error: Check JTAG interface, timings, target power, etc.

Error: Trying to use configured scan chain anyway...

Error: k10.cpu: IR capture error; saw 0x00 not 0x01

Is someone have an idea to manage this issue ?

Thanks in advance

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,232 Views
gfritz
Contributor II

Hi,

Thank you for your answer. We found yesterday the problem : we forgot pull-up on NMI pin (PTA4, pin54 for K10FN1M0xxx12)...

Thank you also for your kind proposition of help

View solution in original post

0 Kudos
Reply
2 Replies
2,232 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you provide the K10 JTAG related circuit?

If yes, we could check the K10 JTAG related schematics.

Customer also could check TWR-K20D50M board schematics about JTAG related circuit design.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,233 Views
gfritz
Contributor II

Hi,

Thank you for your answer. We found yesterday the problem : we forgot pull-up on NMI pin (PTA4, pin54 for K10FN1M0xxx12)...

Thank you also for your kind proposition of help

0 Kudos
Reply