The VBAT pin in the KM34

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The VBAT pin in the KM34

1,355件の閲覧回数
小勇邹
Contributor II

I do not use VBAT in my project. So I connect the VBAT pin to ground.

But I want to use the external 32K for the AFE.

Now I find that the external 32K cannot be initialized.It always stays in the function " PLL_Enable (PLL32KREF_SRC1); ".

Is it affected by the VBAT pin connected to ground?

ラベル(1)
0 件の賞賛
返信
1 返信

1,223件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below KM34 block diagram, the 32K OSC was powered from VBAT pin.

pastedImage_1.png

Thank you for the attention.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信