The VBAT pin in the KM34

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The VBAT pin in the KM34

1,347 Views
小勇邹
Contributor II

I do not use VBAT in my project. So I connect the VBAT pin to ground.

But I want to use the external 32K for the AFE.

Now I find that the external 32K cannot be initialized.It always stays in the function " PLL_Enable (PLL32KREF_SRC1); ".

Is it affected by the VBAT pin connected to ground?

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below KM34 block diagram, the 32K OSC was powered from VBAT pin.

pastedImage_1.png

Thank you for the attention.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply