The Low-Power Timer in the KM34

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The Low-Power Timer in the KM34

2,396 次查看
小勇邹
Contributor II

Hi,

I want to use the Low-Power Timer as a period timer in my application.After setting the value of the register LPTMR_CMR, is there any formula to caculate the period time??How to caculate  it??

标签 (1)
0 项奖励
回复
3 回复数

2,261 次查看
mjbcswitzerland
Specialist V

Hi

The value of the delay (in seconds) is
#define LPTMR_S_DELAY(s_delay) (s_delay * LPTMR_CLOCK) - 1)
whereby the value of LPTMR_CLOCK depends on where you configure it to be taken from; it can be 1000 (LPO), 32768Hz, 4Meg or 32kHz MCGIRCLK, external clock value or external clock value divided by a prescaler.

Regards

Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html

0 项奖励
回复

2,261 次查看
小勇邹
Contributor II

Hi,

Thank you.

What is the minimum value of the period time? Is it possible to set the period as 1us?

0 项奖励
回复

2,261 次查看
mjbcswitzerland
Specialist V

The minimum delay depends on your clock.
If you use the LPO (1kHz) the minimum delay is 1ms (with value of 0)
If you use the 4MHz IRC you can set 250ns steps - 1us would be a value of 3 in this case.

Regards

Mark

0 项奖励
回复