TWR k53n512 need help

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR k53n512 need help

1,751 次查看
alexandro
Contributor I

TWR k53n512

Hey my name is Alex and i am new to the tower system,i was running the tower but it seems like there are pins everywhere on and off. I recently got it from a friend but seem like he was struggling so i wanted to learn it. Does it matter where all the pins lay if i wanted to test the installation instructions to make sure is running well.

标记 (2)
0 项奖励
回复
3 回复数

1,554 次查看
toñohernández
Contributor III

hi Alex:

Welcome to the Tower Geeks world!

Regarding your inquiries:

Not sure if you have checked the TWR-K53N512 Quick Start Guide, it is quite a good option to begin.

Also the TWR-K53N512 User Manual can help with your question (Check the "Input/Output Connectors and Ping Usage Table" in page 18)

Let me know if those help

1,554 次查看
leec
Contributor I

TWR-K53N512 User Manual link is dead (404). :smileycry:

0 项奖励
回复

1,554 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Lee Courtney:

The link is just missing the .pdf extension. More documentation and useful materials are available in the TWR-K53 board and K53 MCU product pages:

Kinetis K53 Tower System Module|Freescale

K53_100 |Kinetis K53 100 MHz MCUs|Freescale

Regards!

Jorge Gonzalez

0 项奖励
回复