TWR k53n512 need help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR k53n512 need help

2,596件の閲覧回数
alexandro
Contributor I

TWR k53n512

Hey my name is Alex and i am new to the tower system,i was running the tower but it seems like there are pins everywhere on and off. I recently got it from a friend but seem like he was struggling so i wanted to learn it. Does it matter where all the pins lay if i wanted to test the installation instructions to make sure is running well.

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,399件の閲覧回数
toñohernández
Contributor III

hi Alex:

Welcome to the Tower Geeks world!

Regarding your inquiries:

Not sure if you have checked the TWR-K53N512 Quick Start Guide, it is quite a good option to begin.

Also the TWR-K53N512 User Manual can help with your question (Check the "Input/Output Connectors and Ping Usage Table" in page 18)

Let me know if those help

2,399件の閲覧回数
leec
Contributor I

TWR-K53N512 User Manual link is dead (404). :smileycry:

0 件の賞賛
返信

2,399件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Lee Courtney:

The link is just missing the .pdf extension. More documentation and useful materials are available in the TWR-K53 board and K53 MCU product pages:

Kinetis K53 Tower System Module|Freescale

K53_100 |Kinetis K53 100 MHz MCUs|Freescale

Regards!

Jorge Gonzalez

0 件の賞賛
返信