TWR-POS-K81 QSPI FLASH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-POS-K81 QSPI FLASH

4,465 Views
devilavanyaanda
Contributor III

Requirement:    QCB for the QSPI Flash Part no: MT25TL512HBA8E12.

 

Environment:    The TWR-POS-K81 KIT is supplied with a QSPI Flash Part no: MT25TL512HBA8E12. Through the  IAR IDE, using USB-MULTILINK  we are loading PAYMENT DEMO application in TWR-POS-K81 . Payment demo application gets loaded in both internal flash and external QSPI flash memory and PAYMENT DEMO application works fine.

 

What we want to do:

  • We want to load the outputfile, paymentdemo.sb in to the TOWER-POS-K81 board using blhost.exe or mfgtools.exe
  • We understand that in order to do this, first we need to create a qspi_config_block_generation.c containing QCB information suitable for MT25TL512HBA8E12 and compile using CodeBlocksIDE to generate a  qspi_config_block_pos.bin.
  • Using the document Kinetis Bootloader QuadSPI User's Guide paymentdemo.bd is required to be created.
  • Further using the Elftosb.exe and paymentdemo.bd prepared for paymentdemo.srec and qspi_config_block_pos.bin the  paymentdemo.sb shall be created.
  • Further this paymentdemo.sb is loaded into the TOWER-POS-K81 board using blhost.exe or mfgtools.exe

 

What we want:

  • QCB file suitable for MT25TL512HBA8E12

 

Note: We tried to create a QCB file at our end, but unsuccessful.

 

Thank you

0 Kudos
Reply
6 Replies

4,351 Views
nxf58904
NXP Employee
NXP Employee

Hi,

MT25TL512HBA8E12 's difference is flash space , but cmd and main timing sequence is same .

Please have a try .

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,351 Views
devilavanyaanda
Contributor III

 Hello Jianyu,

We changed flash space and tried but still its not working.

Thanks in advance

0 Kudos
Reply

4,351 Views
nxf58904
NXP Employee
NXP Employee

Hi,

https://www.nxp.com/docs/en/user-guide/MBOOTQSPIUG.pdf 

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,351 Views
devilavanyaanda
Contributor III

Hello Jianyu,

We required QCB file suitable for MT25TL512HBA8E12 IC 

In "MBOOTQSPIUG.pdf" document the QCB for MT25TL512HBA8E12 IC  is not mentioned.

Thanks in advance

0 Kudos
Reply

4,351 Views
nxf58904
NXP Employee
NXP Employee

Refer this link https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true ,chapter 3.3.3,please have a try .

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,351 Views
devilavanyaanda
Contributor III

Hi Jianyu,

This above link is directing to the below link 

Software | NXP

 we are unable to refer chapter 3.3.3, Please Mention the Document name.

Thanks in advance

0 Kudos
Reply