TWR-KV58F220M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-KV58F220M

2,248件の閲覧回数
liuzhonghuiliu
Contributor II

MBED drive no showing

0 件の賞賛
返信
2 返答(返信)

2,166件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Dear liuzhonghui liu,


Please check the state of your device by refer: DAPLink bootloader update.
If it's in corrupted state. Then you can recover the board by updating the debug interface firmware again.
If it's in bricked state. Then you can only recover the board by flashing a new bootloader with an external debug probe.

Here the TWR-KV58F220M is not in the list of table.
Considering that the OpenSDA versions of the FRDM-K22F and TWR-KV58F220M boards are both V2.1, customer can direct use the file of FRDM-K22F.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,166件の閲覧回数
liuzhonghuiliu
Contributor II

hi Robin_Shen:

the Trouble is  resolved!

Thank you!

Best Regards

liuzhonghui

0 件の賞賛
返信