TWR-KV58F220M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KV58F220M

2,246 Views
liuzhonghuiliu
Contributor II

MBED drive no showing

0 Kudos
Reply
2 Replies

2,164 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Dear liuzhonghui liu,


Please check the state of your device by refer: DAPLink bootloader update.
If it's in corrupted state. Then you can recover the board by updating the debug interface firmware again.
If it's in bricked state. Then you can only recover the board by flashing a new bootloader with an external debug probe.

Here the TWR-KV58F220M is not in the list of table.
Considering that the OpenSDA versions of the FRDM-K22F and TWR-KV58F220M boards are both V2.1, customer can direct use the file of FRDM-K22F.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,164 Views
liuzhonghuiliu
Contributor II

hi Robin_Shen:

the Trouble is  resolved!

Thank you!

Best Regards

liuzhonghui

0 Kudos
Reply