TWR-KM34Z75M Maintenance mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KM34Z75M Maintenance mode

Jump to solution
4,384 Views
KKR231
Contributor II

 

Hi

In my TWR-KM34Z75M board goes into maintenance mode. I erase memory using J-Link but when I press reset button again it goes into maintenance mode. For that what I have to do?

Thankyou

0 Kudos
Reply
1 Solution
4,239 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I confirm each board has the same debugger on the board MK20, but could you try with the J-Link driver?

SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace

Pavel_Hernandez_0-1727216503409.png

Pavel_Hernandez_1-1727216511671.png

Best regards,
Pavel

 

View solution in original post

0 Kudos
Reply
5 Replies
4,364 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your information, and the mode of Maintenance Mode sometimes is when the MK20 (debugger) of the frdm is prepared to update the firmware.

*So, this thread could help you the debugger on the board, to get out of the maintenance mode.

OpenSDA Serial and Debug Adapter | NXP Semiconductors

Best regards,
Pavel

0 Kudos
Reply
4,347 Views
KKR231
Contributor II

Thankyou @Pavel_Hernandez for your response,

But in given link there is files for TWR-KM34Z50M and I required for TWR-KM34Z75M. 

 

0 Kudos
Reply
4,334 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, do not worry you could use the same firmware because the debugger on the board should be the same.

Could you try it? let me know if have more doubts.

Best regards,
Pavel

0 Kudos
Reply
4,290 Views
KKR231
Contributor II

Hello @Pavel_Hernandez 

I tried steps which is given in OpenSDA Serial and Debug Application and I successfully upload that cmsis-dap .bin files in bootloader section of my board. But when I reconnect and use MCUXPresso, board is not shown (PFA) as well as board is not came from maintenance board. 

After I came into bootloader section that copy files are not shown.

Screenshot 2024-09-23 101945.png

 

 

0 Kudos
Reply
4,240 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I confirm each board has the same debugger on the board MK20, but could you try with the J-Link driver?

SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace

Pavel_Hernandez_0-1727216503409.png

Pavel_Hernandez_1-1727216511671.png

Best regards,
Pavel

 

0 Kudos
Reply