TWR-K64F120 can not be connected?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K64F120 can not be connected?

1,036 Views
danielchai
Senior Contributor I

Hi all,

I just got a TWR-K64F120 for the larger RAM.

I installed the Freescale_MQX_4_0_TWRK64F120M.

When I try to download the hello sample code to it through OpenSDA, it does not work.

When I checked the OpenSDA information, it shows

pastedImage_0.png

From the link First Steps with the Freescale TWR-K64F120M | MCU on Eclipse, I also tried connect J39, but it still does not work.

Then I tried to use the Multilink Universal Debugger, no matter with J39 and J16 connected or not, it shows

pastedImage_2.png

and sometime the power LED is not on the LED D3 is blinking.

I am confused.

Any one has some ideas about this?

Thank you.

-Daniel

0 Kudos
Reply
1 Reply

759 Views
mjbcswitzerland
Specialist V

Hi

I would check that the OpenSDA software installed is correct for debugging.

Go to the P&E site and download the latest Pemicro OpenSDA debug update apps: P&E Microcomputer Systems

There is one for your board called MSD-DEBUG-TWR-K64F120_Pemicro_v114.SDA and if you upgrade to this one (according to the details on that page) you may find it then works.

For some reason the boards are delivered with a Mass Storage loader programmed (it does say Mass Storage / Debug App above but I don't think that it means that it can be used as debugger (?). I have about 10 boards with OpenSDA and had to reprogram all of them first to be able to work with the debugger - after programming (which is thankfully simple) all worked fine.

Note for people who use Rowely Crossworks: this IDE used CMSIS-DAP_OpenSDA.S19 which is contained in contained in the KL25 quickstart package - see FRDM-KL25Z: Freescale Freedom Development Platform for Kinetis KL14/15/24/25 MCUs I believe the single file is suitable for all processors (but not fully sure at the moment since I only tested it on the KL25 'till now).

Regards

Mark

0 Kudos
Reply