TWR-K40X256 Software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K40X256 Software

3,051 Views
andreaalvarado
Contributor I

Hello!!

Im trying to install the software for the TWR-K40X256, but in the web says that the page is not found, ive tried with the CD available with the K-40, but there is no JTAG or any other open source program....  can somebody help? im first time user... thanks in advance!!

0 Kudos
Reply
3 Replies

2,823 Views
andreaalvarado
Contributor I

Hello!!

Thanks very much for the response!!

Its my first time so im not sure which program in specific, but ive seen that i need the OSJTAG, or more especifically the P&E Kinetis Tower Toolkit, so i could get the terminal utility and i could program? 

0 Kudos
Reply

2,822 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Andrea,

 

Please take a look to the section 3 on the attached quick start guide for information on how to update the OSBDM/OSJTAG in the board. For example projects, I would recommend you to download the MCUXpresso SDK package for the MK40DX256xxx10:

pastedImage_1.png

Here are some links with more information about the MCUXpresso Config Tools:

MCUXpresso Config Tools is now available!  

Generating a downloadable MCUXpresso SDK v.2 package 

Please notice that the TWR-K40X256 board is not directly supported, the MK40DX256xxx10 devices are supported trough the TWR-K60D100M board so you will have to modify the board.c and board.h files to match the TWR-K40X256 hardware.

 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,822 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Andrea,

Which software are you trying to download?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply