SysTick Timer gives error of 5 second per minute KE02 Micro-controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SysTick Timer gives error of 5 second per minute KE02 Micro-controller

跳至解决方案
2,864 次查看
xpress_embedo
Contributor II

Hello Everyone.

I am using Freescale MKE02Z32xxx4 micro-controller for one of my project, and everything works fine, the complete project is running fine. But my customer reports an issue, that the time taken for executing 10 minute cycle is longer than 10 minutes.

I checked it and found that 1 minute is acting a 1 minute 5 seconds, which means that, something i missed which is causing this behavior.

I am using SysTick to generate 1ms interrupt and using that I am checking timings required ( Example 10 minutes ).

The following is the initialization code.

void Timer_Init( void )
{
SysTick->LOAD = 20000u-1u;
SysTick->VAL = 0;
SysTick->CTRL |= SysTick_CTRL_CLKSOURCE_Msk;
SysTick->CTRL |= SysTick_CTRL_TICKINT_Msk;
}

This function will start the timer.

void Timer_start( void )
{
SysTick->CTRL |= SysTick_CTRL_ENABLE_Msk;
SysTick->LOAD = 20000u-1u;
}

And the priority for the interrupt is 1, second highest.

I am using the the FEI mode.

Capture.PNG

Can anyone tell me what mistake i had done, and how can I correct it.

Please let me know if any other input is required from my side.

Thanks in Advance.

标记 (2)
0 项奖励
回复
1 解答
2,684 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Arun,

The default frequency of Slow internal reference clock may error in CodeWarrior10.7 with Processor Expert.

After input 31.25kHz for factory trimmed IRC, we can see the frequency of Core.

KE02 CW10.7 PE 31.25kHz.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
2,684 次查看
xpress_embedo
Contributor II

Actually I am new to this micro-controller and after using CodeWarrior, I cam to know that the clock is around 16.66MHz and after updating that values, system works properly with correct timings.

0 项奖励
回复
2,685 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Arun,

The default frequency of Slow internal reference clock may error in CodeWarrior10.7 with Processor Expert.

After input 31.25kHz for factory trimmed IRC, we can see the frequency of Core.

KE02 CW10.7 PE 31.25kHz.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,684 次查看
xpress_embedo
Contributor II

Thanks Robin.

Can you help me in code protection for KE02 series.

I am using IAR and I don't understand how can I protect my code.

It looks like that the Mass Protection is always enabled for this series of micro-controller (MKE02Z32xxx4).

So even if I accidentally secured the flash I can re-flash. Is it right??

I think it's better if I open a new thread for this.

0 项奖励
回复
2,684 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

You can mass erase the flash and then re-flash it. And please refer the method in 'Flash protection with IAR'.

8.2 Flash security.jpg

0 项奖励
回复