Stuck at Starting target CPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stuck at Starting target CPU

3,270件の閲覧回数
trilokjt
Contributor III

Hi Everyone,

I'm trying to create new Project using KDS ( Using KSDK 1.2.0), I have done Proper Clock and CPU settings and generated PE Code. But I'm unable to enter main of the program, I  always gets stuck at Starting target CPU it wont move further . Please help out

Processor :  MK60DN512VMD10

JTAG :         J-Link Segger

IDE     :          

Kinetis Design Studio

Version: 3.2.0

Thank you/ Regards

Trilok

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,660件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Trilok,

I recommand you use the examples in KSDK2.0. (If you have not used it, please read Introducing Kinetis SDK v2 first.)

You can download and install it refer the methods in How to: install KSDK 2.0.

Select MK60DN512xxx10 configuration.png

Best Regards,

Robin

0 件の賞賛
返信

2,660件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Trilok,

Thank you for interest in NXP Semiconductor products and the opportunity to serve you.

I was wondering if you can share the demo, then I can replicate the issue on my site.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信