Speed of switching Ouputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Speed of switching Ouputs

829 次查看
Jmir
Contributor II

I have tested the maximum switching frequency of the ports in MKE15Z7. For this I used an FTM with an output signal placed on one of the doors. With the clock frequency of the module at 72Mhz I managed to reach up to 3Mhz at the port with a reasonable signal.

Is it possible to further increase the frequency of the output signal while maintaining the electrical characteristics?

0 项奖励
回复
1 回复

823 次查看
myke_predko
Senior Contributor III

@Jmir 

I think the short answer is "No".  

We had a discussion regarding ths a couple of months or so about it and there are a lot of reasons why direct DO is limited to 100s if kHz when you want to do something intelligent.  If it's a repeating signal, there are tricks like using the SPI ports that will give you speeds up to 10Mbps or so.

What are you trying to do?

myke

0 项奖励
回复