Signal graph with eGUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Signal graph with eGUI

ソリューションへジャンプ
2,448件の閲覧回数
elisamejia
Contributor III

Hi all,

I need to graph a sinusoidal signal using the graph object from eGUI. I'm using the TWR-LCD-RGB and the TWR-K70 module.

What I'm doing is using the ADC0 and acquiring the sinusoidal from a function generator. I acquire the data and then convert it to float after mapping the acquired data. According to what I've found I need to add data to the traces of the graph, the format of this data being D4D_GRAPH_VALUE, but apparently the D4D_GRAPH_VALUE data type retrieves integers and no float values.

What should I do to graph the sinusoidal signal?

Thanks in advance,

Elisa

タグ(2)
0 件の賞賛
返信
1 解決策
1,876件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Elisa,

Did the answer from Luis Casado in the thread below answer your question?

Re: eGUI 3.0 demo on TWR-LCD-RGB

Best regards,

Earl.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,877件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Elisa,

Did the answer from Luis Casado in the thread below answer your question?

Re: eGUI 3.0 demo on TWR-LCD-RGB

Best regards,

Earl.

0 件の賞賛
返信