Signal graph with eGUI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Signal graph with eGUI

Jump to solution
2,417 Views
elisamejia
Contributor III

Hi all,

I need to graph a sinusoidal signal using the graph object from eGUI. I'm using the TWR-LCD-RGB and the TWR-K70 module.

What I'm doing is using the ADC0 and acquiring the sinusoidal from a function generator. I acquire the data and then convert it to float after mapping the acquired data. According to what I've found I need to add data to the traces of the graph, the format of this data being D4D_GRAPH_VALUE, but apparently the D4D_GRAPH_VALUE data type retrieves integers and no float values.

What should I do to graph the sinusoidal signal?

Thanks in advance,

Elisa

Tags (2)
0 Kudos
Reply
1 Solution
1,845 Views
EarlOrlando
Senior Contributor II

Hello Elisa,

Did the answer from Luis Casado in the thread below answer your question?

Re: eGUI 3.0 demo on TWR-LCD-RGB

Best regards,

Earl.

View solution in original post

0 Kudos
Reply
1 Reply
1,846 Views
EarlOrlando
Senior Contributor II

Hello Elisa,

Did the answer from Luis Casado in the thread below answer your question?

Re: eGUI 3.0 demo on TWR-LCD-RGB

Best regards,

Earl.

0 Kudos
Reply