Serial_LDD - impossible to receive characters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial_LDD - impossible to receive characters

ソリューションへジャンプ
2,679件の閲覧回数
remibeges
NXP Employee
NXP Employee

I cannot seem to get the Serial_LDD module to receive any characters.

What bothers me is that I've set a breakpoint in the Event.c onBlockReceive interrupt, but the program NEVER reaches it. I have tried arduino console, putty, python for sending serial characters, checked the serial port a hundred times, doesn't seem related to the computer.

Main.c:

/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/

  PE_low_level_init();

  /*** End of Processor Expert internal initialization.                    ***/

  /* Write your code here */

  /* For example: for(;;) { } */

  set_serial_state(FALSE);

  uint8_t data[10];

  AS1_ReceiveBlock(AS1_DeviceData, data, 1);

  for(;;)

  {

        if(get_serial_state())

        {

             // Send it back

             AS1_SendBlock(AS1_DeviceData, data, 1);

             set_serial_state(FALSE);

        }

  }

functions.h

#ifndef SOURCES_FUNCTIONS_H_

#define SOURCES_FUNCTIONS_H_

#include "PE_Types.h"

extern bool serial_rx_state;

void set_serial_state(bool state);

bool get_serial_state();

#endif /* SOURCES_FUNCTIONS_H_ */

functions.c

bool serial_rx_state;

void set_serial_state(bool state)

{

  serial_rx_state = state;

}

bool get_serial_state()

{

  return serial_rx_state;

}

And the interrupt in Events.c

void AS1_OnBlockReceived(LDD_TUserData *UserDataPtr)

{

/* Write your code here ... */

  set_serial_state(TRUE);

}

If somebody can hint me why it's not working, I would appreciate it because I'm completely stuck. I'm just stunned that this simple code won't simply work. I'm using KDS 3.00 and KL26Z

BTW the documentation of the serial_ldd component seems out of date, it is referring to a ProcessorExpert.c file, but I cannot find this file anywhere in the hierarchy.

PS : No block code in this online editor ??

EDIT : I cannot even send characters now

Main .c

* Write your code here */

  /* For example: for(;;) { } */

  set_serial_state(FALSE);

  uint8_t data[10];

  AS1_ReceiveBlock(AS1_DeviceData, data, 1);

  uint32_t i = 0;

while(1)

  {

   if(i >= 10000)

   {

   data[0] = "o";

   data[1] = "k";

   AS1_SendBlock(AS1_DeviceData, data, 2);

   i = 0;

   }

   else

   i++;

  }

I receive strictly nothing. Also checked speed (9600 bauds), same on both sides. This is starting to be very frustrating

ラベル(1)
0 件の賞賛
返信
1 解決策
2,425件の閲覧回数
remibeges
NXP Employee
NXP Employee

it is done in PE_low_level_init

Untitled.png

Is there anything else to activate transmitter and emitter ?

EDIT :

I forgot to check transmitter and emitter pins, for using KL26Z usb serial I think they were wrong by default.

I think the following pins are right :

Receiver : TSI0_CH2/PTA1/UART0_RX/TPM2_CH0

Transmitter : TSI0_CH3/PTA2/UART0_TX/TPM2_CH1

I'll edit once I tested that

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,425件の閲覧回数
lategoodbye
Senior Contributor I

Is initialization done by PE_low_level_init() or by separate AS1_Init() ?

Do you enable receiver and transmitter in Processor expert?

0 件の賞賛
返信
2,426件の閲覧回数
remibeges
NXP Employee
NXP Employee

it is done in PE_low_level_init

Untitled.png

Is there anything else to activate transmitter and emitter ?

EDIT :

I forgot to check transmitter and emitter pins, for using KL26Z usb serial I think they were wrong by default.

I think the following pins are right :

Receiver : TSI0_CH2/PTA1/UART0_RX/TPM2_CH0

Transmitter : TSI0_CH3/PTA2/UART0_TX/TPM2_CH1

I'll edit once I tested that

0 件の賞賛
返信
2,425件の閲覧回数
remibeges
NXP Employee
NXP Employee

OK now I can send characters appropriately. I also solved my initial issue, the mcu never seemed to receive the incoming characters because I am using the MULT2B sensor shield that hosts a bluetooth module. This module will capture any incoming data on the openSDA port, that will not be forwarded to the MCU. And thus the MCU will never see this data if connected by USB cable. Once I removed the shield, the MCU behaved as expected.

0 件の賞賛
返信