SPI Communication using Multiple Ports Simultaneously

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Communication using Multiple Ports Simultaneously

1,479 次查看
eosweeny
Contributor I

The Kinetis K64F Sub-Family Data Sheet (https://www.nxp.com/docs/en/data-sheet/K64P144M120SF5.pdf) lists that there are 3 SPI communication interfaces available. Is it possible to use these interfaces simultaneously?

标签 (1)
0 项奖励
回复
1 回复

1,467 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Sure.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复