SPI Communication using Multiple Ports Simultaneously

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Communication using Multiple Ports Simultaneously

1,484 Views
eosweeny
Contributor I

The Kinetis K64F Sub-Family Data Sheet (https://www.nxp.com/docs/en/data-sheet/K64P144M120SF5.pdf) lists that there are 3 SPI communication interfaces available. Is it possible to use these interfaces simultaneously?

Labels (1)
0 Kudos
Reply
1 Reply

1,472 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Sure.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply