SMBus Address Resolution Protocol support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SMBus Address Resolution Protocol support

ソリューションへジャンプ
4,849件の閲覧回数
severinjdavis
NXP Employee
NXP Employee

SMBus ARP requires slaves to arbitrate after receiving general "get UDID" command. Without this slave arbitration, address assignment isn't possible via ARP.

We have a master requesting information from multiple kinetis slaves with the same address, and the received data is an AND of the slaves' sent information. This indicates that slave arbitration is not happening, as the first 0 should have caused at least one slave to drop out. Instead, all continue transmitting, resulting in a bitwise AND.

The reference manual claims support for SMBus version 2.0. Version 2.0 includes ARP.

So it seems as though SMBus 2.0 is supported, except for ARP.

Am I correct here?

タグ(4)
0 件の賞賛
返信
1 解決策
4,006件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Severin Davis:

The I2C module in Kinetis complies with SMBUS specification, but it is a fixed not discoverable device. So your understanding is correct, the slaves do not arbitrate, instead they talk at the same time over the bus.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,007件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Severin Davis:

The I2C module in Kinetis complies with SMBUS specification, but it is a fixed not discoverable device. So your understanding is correct, the slaves do not arbitrate, instead they talk at the same time over the bus.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信