SDRAM and NOR flash/QSPI flash interface in MK22FN512VLL12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDRAM and NOR flash/QSPI flash interface in MK22FN512VLL12

1,213 次查看
prasannanaik
Contributor III

Hi,

   Can SDRAM and NOR/QSPI flash be interfaced with MK22FN512VLL12 through Flex memory interface?

Thanks and best regards,

Prasanna

标签 (1)
0 项奖励
回复
1 回复

1,126 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Prasanna Naik,

   1. SDRAM for K22, you can use the flexbus interface

   More details, you can refer to this post:

Flexbus and SDRAM Multiplex on K65F_169GBA 

  And an5095:

http://cache.nxp.com/files/32bit/doc/app_note/AN5095.pdf 

   2. QSPI for K22

    Unfortuntatly, MK22FN512VLL12  doesn't have the QSPI interface, maybe you just can use the SPI interface.

   Flex memory is just used for the internal memory, it can't be used to the external memory.

Wish it helps you!

Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复