SDIO block transfers stop too soon

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDIO block transfers stop too soon

ソリューションへジャンプ
3,072件の閲覧回数
gnate
Contributor III

I'm working with the MK64FN1M and I am having issues with SDIO block transfers using CMD53 (command).  Up till now I have had no problems sending commands and byte transfers.  I am using 1-bit at 400 KHz baud, 1 block, 128 bytes, 128 >> 2 for the watermark, and card detect disabled on both ends.

I've connected a scope and can confirm that data is being sent and received on the SDIO DAT0 pin.  I can also confirm that the command sent is correct on the command pin and that the data transmitted or received is the correct binary data that I am sending or expecting to receive.

The issue is that the data being sent is only around 14 bytes + the 2 byte CRC.  When receiving data, again, the clock only runs long enough to receive 16 bytes and afterwards the IC holds the data line low.

Is this a flaw in the MK64FN1M0VLL12?  Am I missing anything or is there a workaround?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,860件の閲覧回数
gnate
Contributor III

DRAT!  Mistakenly had the MCU configured for 4-pin and the IC configured for 1-pins.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,860件の閲覧回数
chaoxu
Contributor I

Hi, Nate Sigrist. 

I'm working with the MK60DN512ZVLQ10 and I am having troubles with SDIO block transfers using CMD53 (command). The Problem is that when I send CMD53 for block transfers, the device can't return the data. However, I can use CMD52 to read/write single data successfully. Could you send me your sdio.c/sdio.h file as reference?Thank you very much.

My e-mail is [email protected].

0 件の賞賛
返信
2,860件の閲覧回数
gnate
Contributor III

Here is a screen shot of MK64FN1M0VLL12 sending a block read request to an IC followed by the IC sending block data over the data line (green)

tek00000.png

Here is a screen shot of the MK64FN1M0VLL12 sending a block write request to an IC followed by the MCU sending block data over the data line (green)

tek00001.png

2,861件の閲覧回数
gnate
Contributor III

DRAT!  Mistakenly had the MCU configured for 4-pin and the IC configured for 1-pins.

0 件の賞賛
返信