SDIO block transfers stop too soon

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO block transfers stop too soon

Jump to solution
3,158 Views
gnate
Contributor III

I'm working with the MK64FN1M and I am having issues with SDIO block transfers using CMD53 (command).  Up till now I have had no problems sending commands and byte transfers.  I am using 1-bit at 400 KHz baud, 1 block, 128 bytes, 128 >> 2 for the watermark, and card detect disabled on both ends.

I've connected a scope and can confirm that data is being sent and received on the SDIO DAT0 pin.  I can also confirm that the command sent is correct on the command pin and that the data transmitted or received is the correct binary data that I am sending or expecting to receive.

The issue is that the data being sent is only around 14 bytes + the 2 byte CRC.  When receiving data, again, the clock only runs long enough to receive 16 bytes and afterwards the IC holds the data line low.

Is this a flaw in the MK64FN1M0VLL12?  Am I missing anything or is there a workaround?

Tags (3)
0 Kudos
Reply
1 Solution
2,946 Views
gnate
Contributor III

DRAT!  Mistakenly had the MCU configured for 4-pin and the IC configured for 1-pins.

View solution in original post

0 Kudos
Reply
3 Replies
2,946 Views
chaoxu
Contributor I

Hi, Nate Sigrist. 

I'm working with the MK60DN512ZVLQ10 and I am having troubles with SDIO block transfers using CMD53 (command). The Problem is that when I send CMD53 for block transfers, the device can't return the data. However, I can use CMD52 to read/write single data successfully. Could you send me your sdio.c/sdio.h file as reference?Thank you very much.

My e-mail is [email protected].

0 Kudos
Reply
2,946 Views
gnate
Contributor III

Here is a screen shot of MK64FN1M0VLL12 sending a block read request to an IC followed by the IC sending block data over the data line (green)

tek00000.png

Here is a screen shot of the MK64FN1M0VLL12 sending a block write request to an IC followed by the MCU sending block data over the data line (green)

tek00001.png

2,947 Views
gnate
Contributor III

DRAT!  Mistakenly had the MCU configured for 4-pin and the IC configured for 1-pins.

0 Kudos
Reply