SDIO block transfers stop too soon

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDIO block transfers stop too soon

跳至解决方案
2,012 次查看
gnate
Contributor III

I'm working with the MK64FN1M and I am having issues with SDIO block transfers using CMD53 (command).  Up till now I have had no problems sending commands and byte transfers.  I am using 1-bit at 400 KHz baud, 1 block, 128 bytes, 128 >> 2 for the watermark, and card detect disabled on both ends.

I've connected a scope and can confirm that data is being sent and received on the SDIO DAT0 pin.  I can also confirm that the command sent is correct on the command pin and that the data transmitted or received is the correct binary data that I am sending or expecting to receive.

The issue is that the data being sent is only around 14 bytes + the 2 byte CRC.  When receiving data, again, the clock only runs long enough to receive 16 bytes and afterwards the IC holds the data line low.

Is this a flaw in the MK64FN1M0VLL12?  Am I missing anything or is there a workaround?

标记 (3)
0 项奖励
回复
1 解答
1,800 次查看
gnate
Contributor III

DRAT!  Mistakenly had the MCU configured for 4-pin and the IC configured for 1-pins.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,800 次查看
chaoxu
Contributor I

Hi, Nate Sigrist. 

I'm working with the MK60DN512ZVLQ10 and I am having troubles with SDIO block transfers using CMD53 (command). The Problem is that when I send CMD53 for block transfers, the device can't return the data. However, I can use CMD52 to read/write single data successfully. Could you send me your sdio.c/sdio.h file as reference?Thank you very much.

My e-mail is andy_xuchao@163.com.

0 项奖励
回复
1,800 次查看
gnate
Contributor III

Here is a screen shot of MK64FN1M0VLL12 sending a block read request to an IC followed by the IC sending block data over the data line (green)

tek00000.png

Here is a screen shot of the MK64FN1M0VLL12 sending a block write request to an IC followed by the MCU sending block data over the data line (green)

tek00001.png

1,801 次查看
gnate
Contributor III

DRAT!  Mistakenly had the MCU configured for 4-pin and the IC configured for 1-pins.

0 项奖励
回复