SD support on FRDM-K22F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD support on FRDM-K22F

1,269 Views
davepfaltzgraff
Senior Contributor I

Is there a plan to support the FAT file system on the SD interface on the FRDM-K22F platform? (This can be either stand-alone or as part of the MQX package.)

I understand the limitation of not having the HD interface (one data line versus four), but I don't need the speed - just a basic interface for logging, etc.

If the support is there now and I'm just not looking at the right places, some pointers on the implementation would be great.

Thanks.

0 Kudos
Reply
1 Reply

1,152 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David,

I've not found the demo that integrated with filesystem so far and I'll contact with KSDK team to confirm it later.

However I'd like to recommend two practical experiments about SD and I think they're worth to refer to.

FatFs with Kinetis | MCU on Eclipse

Multi-Drive Support with FatFS | MCU on Eclipse
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply