Running KL03 without an Xtal OSC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running KL03 without an Xtal OSC

931 次查看
tedmawson
Contributor III

I'm trying to use a MKL03Z32CAF4R without a crystal.  The KSDK doumentation says "MCG uses the OSC as an external reference clock source." Does this mean is can use it as a reference of it needs it as a reference?

If it IS OK to run MCG lite without any OSC, what accuracy will I get asking for 2 MHz clock from it?

标记 (1)
0 项奖励
回复
1 回复

802 次查看
dereksnell
NXP Employee
NXP Employee

Hi Ted,

Yes, you can use the internal oscillators to clock the MCU without needing an external crystal.  Below is the Clocking Diagram of the MCU from the KL03 reference manual.

And the datasheet contains the accuracy of the internal oscillators.  See the snipped below for the 2MHz IRC.

Clocking Diagram.jpg

IRC2M.jpg

0 项奖励
回复