Running KL03 without an Xtal OSC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running KL03 without an Xtal OSC

1,343 Views
tedmawson
Contributor III

I'm trying to use a MKL03Z32CAF4R without a crystal.  The KSDK doumentation says "MCG uses the OSC as an external reference clock source." Does this mean is can use it as a reference of it needs it as a reference?

If it IS OK to run MCG lite without any OSC, what accuracy will I get asking for 2 MHz clock from it?

Tags (1)
0 Kudos
Reply
1 Reply

1,214 Views
dereksnell
NXP Employee
NXP Employee

Hi Ted,

Yes, you can use the internal oscillators to clock the MCU without needing an external crystal.  Below is the Clocking Diagram of the MCU from the KL03 reference manual.

And the datasheet contains the accuracy of the internal oscillators.  See the snipped below for the 2MHz IRC.

Clocking Diagram.jpg

IRC2M.jpg

0 Kudos
Reply