Reset problem with K02FN128VLH10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset problem with K02FN128VLH10

1,464件の閲覧回数
michalpokorny
Contributor I

Dear Madam or Sir,

I have hardware problems with the K02FN128VLH10 unfortunately. If I connected the Segger J-link debugger, the application works and the signal Reset has logical 1 level. If I disconnected the debugger and toggle the DC power supply then the application stop running and the Reset pin generate pulses with 10 kHz period approximately. The empty microcontroller generates nothing. I am not sure if it is a hardware or software mistake.  I use the standard startup library from the Kinetis studio 2.0 and the developed application works with FRDM-K22F without problem. Really thank you in advance for your help. Your sincerely Michal Pokorny

ラベル(1)
0 件の賞賛
返信
1 返信

1,277件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Michal,

I found your submit the same issue at below thread, please check my feedback at that thread.

Thank you for the understanding.

https://community.freescale.com/thread/353315


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信