Recieve USB keyboard data - USB Host Demo?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Recieve USB keyboard data - USB Host Demo?

跳至解决方案
1,544 次查看
stevenlutz
Contributor III

I'm new to developing with USB and I'm hoping someone can recommend a demo that will take a USB Keyboard as input for either the FRDM-K22F or FRDM-KL25Z

Thank you

 

0 项奖励
回复
1 解答
1,524 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @stevenlutz ,

The USB interface in KL27 is device only. It's impossible to connect a USB keyboard.

K22 USB interface is OTG. It can connect a USB device, such as keyboard. Please download FRDM-K22F SDK from https://mcuxpresso.nxp.com/en/welcome. There is a USB host_mouse_keyboard demo in SDK_2.10.0_FRDM-K22F\boards\frdmk22f\usb_examples\usb_host_hid_mouse_keyboard.

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,525 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @stevenlutz ,

The USB interface in KL27 is device only. It's impossible to connect a USB keyboard.

K22 USB interface is OTG. It can connect a USB device, such as keyboard. Please download FRDM-K22F SDK from https://mcuxpresso.nxp.com/en/welcome. There is a USB host_mouse_keyboard demo in SDK_2.10.0_FRDM-K22F\boards\frdmk22f\usb_examples\usb_host_hid_mouse_keyboard.

 

Regards,

Jing

0 项奖励
回复