Recieve USB keyboard data - USB Host Demo?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recieve USB keyboard data - USB Host Demo?

Jump to solution
1,678 Views
stevenlutz
Contributor III

I'm new to developing with USB and I'm hoping someone can recommend a demo that will take a USB Keyboard as input for either the FRDM-K22F or FRDM-KL25Z

Thank you

 

0 Kudos
Reply
1 Solution
1,658 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @stevenlutz ,

The USB interface in KL27 is device only. It's impossible to connect a USB keyboard.

K22 USB interface is OTG. It can connect a USB device, such as keyboard. Please download FRDM-K22F SDK from https://mcuxpresso.nxp.com/en/welcome. There is a USB host_mouse_keyboard demo in SDK_2.10.0_FRDM-K22F\boards\frdmk22f\usb_examples\usb_host_hid_mouse_keyboard.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
1,659 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @stevenlutz ,

The USB interface in KL27 is device only. It's impossible to connect a USB keyboard.

K22 USB interface is OTG. It can connect a USB device, such as keyboard. Please download FRDM-K22F SDK from https://mcuxpresso.nxp.com/en/welcome. There is a USB host_mouse_keyboard demo in SDK_2.10.0_FRDM-K22F\boards\frdmk22f\usb_examples\usb_host_hid_mouse_keyboard.

 

Regards,

Jing

0 Kudos
Reply